Skip to main content
Renesas Electronics America - Knowledgebase

sf_audio_record_i2s Module Guide Resources

Last Updated:02/28/2018


Where can I find the references to module guide resources for the Audio Record i2s Framework  module on sf_audio_record_i2s?


Information on the module guide itself and the associated resources and known issues are available here.


The Audio Record I2S Framework module provides high-level APIs for audio recording applications and uses the I2S interface. The Audio Record I2S Framework module uses the SSI, GPT and DTC peripherals on the Synergy MCU. A user-defined callback can be created to indicate that new samples are stored in the user buffer.

The Audio Record I2S Framework module supports the following features:

  • Thread safe
  • Records data in 8 or 16-bit PCM
  • Periodic callback function when new samples are available
  • Configurable number of samples (sample count) per callback


Module Guide

Currently there is no module guide available for this module.


Module Guide Resources

The following application projects are available from the Renesas web site at the referenced url.

  • Renesas Synergy™ Project DK-S124 Simple Record/Playback here.
  • Messaging Framework Module Guide - Application Project here.


Known issues

  • Refer to the most current SSP release notes for any known issues.
Suitable Products