Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

How do I create a custom Board Support Package (BSP)

Last Updated: 11/20/2015

Question:

How do I create a custom Board Support Package (BSP) for a Synergy project?

Answer:

You can easily create a custom BSP by following the guidelines shown in this application note.

 

  • Was this article helpful?