Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Number of Slots and Subslots TPS-1

Last Updated:06/01/2017

Question:

How many slots and subslots are possible with the TPS-1?

Answer:

The sum of the number of slots and subslots must not be higher than 8 (for example, 4 slots and 4 subslots). Data exchange is only possible in a subslot.
For the local IO interface only one slot/subslot each is possible due to the different operation mode.
Suitable Products
TPS-1
  • Was this article helpful?