Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

TPS-1 2.5ns Internal Time Stamp Resolution

Last Updated:06/01/2017

Question:

How do you get an internal time stamp resolution of 2.5 ns? And how is this measured?

Answer:

An internal PLL generates a 400 MHz clock from which 2.5 ns resolution is derived.
Suitable Products
TPS-1
  • Was this article helpful?