Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Use of TPS-1 Internal CPU

Last Updated:06/01/2017

Question:

Can customers use the internal CPU for PC applications?

Answer:

The internal CPU of the TPS-1 is exclusively reserved for handling the PROFINET stack; all application programs must run on a host CPU. Only in the case of parallel or serial IO-mode will the TPS-1 handle the application as well, though only things such as simple GPIO control.
Suitable Products
TPS-1