Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

What do the symbols of max rating of transistors and FETs represent?

Latest Updated:02/01/2008

Question:

What do the symbols of the absolute maximum ratings of transistors and FETs represent?

Answer:

The symbols mean the following.
In V(1)(2)(3), the symbols stand for the following:

(1) Pin to be measured
(2) Reference pin
(3) Status of connection between the reference pin of (2) and a pin other than the pin of (1) or (2)
S: Short
O: Open
X: Applied specified bias
R: Connected to specified DC resistance
Suitable Products
USB3.0 Host Controller
UPD720202
UPD720201
UPD720200A
UPD720200
USB2.0 Host Controller
UPD720102
UPD720101
UPD720100A