What is the zero-cross frequency of an operational amplifier?
Latest Updated:12/01/2011
Question:
What is the zero-cross frequency of an operational amplifier?
Answer:
The zero-cross frequency is the frequency at which the open loop voltage gain becomes 0 dB (×1) and is calculated from the Aυ vs. f characteristics.
Suitable Products
Operational Amplifiers |
USB2.0 Host/Peripheral Controller |
UPD720150 |