Skip to main content
Renesas Electronics America - Knowledgebase

CAN API and Bus Modes eLearning Course

Last Updated: 06/27/2016


Does Renesas offer a training course on the CAN API?


Renesas is happy to offer this free Renesas Interactive course explaining the features available in most newer CAN peripherals as well as the CAN API firmware. Topics included in this course include an overview of CAN features, mailbox structure, the CAN API and how it simplifies design and development, differences in receiving and polling using Polled vs. Interrupt designs, error handling, and an overview of available test modes.

Note that you will need to sign into your Renesas SSO (Single Sign On) account or complete a free registration to proceed.