Skip to main content
Renesas Electronics America - Knowledgebase

RL78 Timers RD, RG and RJ elearning Course

Last Updated: 06/09/2015


This free course provides an introduction to the RL78s Timer units RD, RG and RJ. Basic functions are reviewed including operating modes (Timer Mode, PWM Mode, Complementary PWM Mode, Phase Counting Mode, Event Counter Mode, etc.) and buffer operations. Several application examples are offered, including motor control.

How to Access

You can access the Renesas Interactive course at the following URL:

Note that you will need to sign into your Renesas SSO (Single Sign On) account or complete a free registration to proceed.

  • Was this article helpful?