Skip to main content
Renesas Electronics America - Knowledgebase

RX Family Overview eLearning Course

Last Updated: 06/28/2016


Does Renesas offer an overview presentation on the 32-bit RX MCU family?


This free Renesas e-Learning course provides an overview of the RX family of 32-bit microcontrollers, highlighting the key benefits of its breakthrough new architecture and showing how the RX can be used to address the demanding requirements in a wide variety of today’s microcontroller, digital signal controller, and digital signal processor applications.
  • Was this article helpful?