Skip to main content
Renesas Electronics America - Knowledgebase

Shipping Containers & Pin 1 Orientation

Last Updated: 07/07/2016


What is the pin 1 orientation of the products within the shipping container? What are the dimensions of the shipping container (tube or tape & reel)


The orientation of pin 1 varies depending on package type and container type (i.e. tray or tape & reel). Please refer to either the List of IC Packages(PKG type) or List of IC Packages(Pin Count). Select the appropriate package type and/or pin count range, then scroll to the corresponding shipping container to find the pin 1 orientation. We encourage you to review both the applicable Container (orange) and Packing (blue) diagrams. Refer to the image below for an example of the information available.packaging_diagrams.jpg