Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Using SQMlint on HEW

Last Updated:02/21/2018

Question:

How do I output a report using SQMlint on HEW?

Answer:

Step 1. Select the HEW menu >> [Build] >> [SuperH RISC engine Standard Toolchain].

Step 2. Then, in the C/C++ tab, select “MISRA C rule check” for [Category].

Step 3. Check option: Select “MISRA1998”
 Note: “MISRA2004” and “Group definition file” are not supported.

Step 4. Show entries for: select “Report”

Step 5. Then, select the “Generate report file” checkbox.

SQMlint.png

Suitable Products
High-performance Embedded Workshop
C/C++ Compiler Package for SuperH Family