What performance do the standard library functions have ?
Latest Updated:10/28/2014
Question:
What performance do the standard library functions have ?
Answer:
The size and performance in execution of the standard libraries is easily measured by using the simulator that comes with the compiler.
If you do not already have the product, download the free evaluation version of the compiler to check the performance of the libraries.
If you do not already have the product, download the free evaluation version of the compiler to check the performance of the libraries.
Suitable Products
CS+ (formerly CubeSuite+) |
High-performance Embedded Workshop |