Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Bluetooth low energy Communication Range

Last Updated:02/13/2017

Question:

What is the typical RF communication range for the RL78/G1D?

Answer:

It is about 15 to 20m based on our evaluations using the RL78/G1D evaluation board outdoors.
However, since the communication range varies depending on the presence or absence of shields and obstacles, placement conditions, surrounding environment, etc., your results may differ.
Suitable Products
RL78/G1D
Bluetooth