Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Flash ROM writing of data during RL78/G1D Operation

Last Updated:02/13/2017

Question:

Is it possible to write user data to flash memory during RL78/G1D operation?

Answer:

It is possible to do so using self programming library (EEPROM emulation library)
1.8V is the minimum input voltage for this operation.
Suitable Products
RL78/G1D
Bluetooth
RL78 Family