Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Connection with a Pairing Completed Remote Device

Last Updated:09/20/2017

Question:

How do I connect with a pairing completed remote device?

Answer:

Use the RBLE_GAP_Create_Connection function to establish a link with the remote device.
The link establishment request by the RBLE_GAP_Create_Connection function continues until the link establishment event RBLE_GAP_EVENT_CONNECTION_COMP is notified or until the request is canceled by the RBLE_GAP_Connection_Cancel function.

It should be noted that the next request cannot be issued while the link establishment request is continuing.

For details, refer to the following manual:

Bluetooth® Low Energy Protocol Stack API Reference Manual: Basics (R01UW0088)
https://www.renesas.com/search/keyword-search.html#q=R01UW0088&genre=document

Suitable Products
RL78/G1D
Bluetooth