Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Power Loss during Over the Air (OTA) Update

Last Updated:02/13/2017

Question:

If a sudden power loss occurs while an Over the Air (OTA) update is in progress, could the Bluetooth low energy communication function of the RL78/G1D be compromised?

Answer:

Over the Air (OTA) firmware updates target the application memory. Since the memory bits storing protocol stack are not accessible via OTA, Bluetooth low energy communication functionality will not be affected.
Suitable Products
RL78/G1D
Bluetooth