Skip to main content
Renesas Electronics America - Knowledgebase

Does Renesas Electronics use same lead-free marking on all products?

Latest Updated:04/01/2007


Does Renesas Electronics use the same lead-free marking on all products?


No, the lead-free marking is not completely the same on all products.
You might expect the lead-free marking to be close to the pin 1 index, but this is not always the case.
The picture below shows an example of a chip on which the markings might be confused.

Some markings are made by using paint, and some by using laser (without any scoops).
The markings are always circular.
Suitable Products