Skip to main content
Renesas Electronics America - Knowledgebase

How can I find out the (MSL) of a product and its definition?

Latest Updated:03/01/2006


How can I find out the moisture sensitivity level (MSL) of a product? Is it defined in any documentation?


The moisture sensitivity level (MSL) as defined by J-STD-020 is not specified for products made by the company formerly known as NEC Electronics.
However, the baking time and the number of storage days after opening the dry pack are defined by the 4.3.2 Heat Resistance Temperature Profile Symbols.
Suitable Products
  • Was this article helpful?