Can unused pins be left open in the output mode?
Latest Updated:12/01/2011
Question:
Regarding the handling method of unused pins of the uPD78F0034, the data sheet describes "Independently connect to VDD0 or VSS0 via a resistor".
Will problems result from handling as "open in the output mode" ?
Will problems result from handling as "open in the output mode" ?
Answer:
While such handling is not totally prohibited, some problems remain.
Please refer to "Handling of unused pins".
Please refer to "Handling of unused pins".
Suitable Products
RL78 Family |
78K Family |