Skip to main content
Renesas Electronics America - Knowledgebase

Why does oscillation of main clock stops even if it's not on STOP mode?

Latest Updated:04/01/2006


Oscillation of the main clock stops even though I have not executed a STOP instruction.
I do not think there is a problem with the program as it has already been checked using an emulator.


Is there oscillator matching?
Normal oscillation cannot be obtained unless there is oscillator matching.
Suitable Products
RL78 Family
78K Family