Does the time of the clock need to be set every time the power is turn on?
Latest Updated:05/28/2013
Question:
Does the time of the real-time clock need to be set every time the power is turned on?
Answer:
Yes, the time needs to be set every time the power is turned on.
*In the RX630/RX631/RX63N Groups, the time does not have to be set again when power is turned on from VBATT operation, because the RTC operates continuously.
Suitable Products
RX62N, RX621 |
RX630 |
RX63N, RX631 |
RX210 |
RX220 |
RX110 |
RX111 |