Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Robust device evaluation environment for improved sensitivity

Last Updated:01/29/2018

Question:

Has the development environment for the RX130 group been prepared?

Answer:

Renesas provides a robust evaluation environment for the new RX130 MCUs to support both self- and mutual-capacity functions.

•A Renesas Starter Kit designed for basic function evaluation

•A Renesas Touch Solution Kit designed for a detailed capacitive touch feature evaluation

•The Workbench6 v1.07.00.00 tool environment with improved noise immunity and tuning ability to improve usability for capacitive touch software development with adding sample project and tuning window etc.

•Development environment toolbox, including Renesas’ FIT, emphasizing portability between MCUs within the RX Family

Suitable Products
RX130