Is data flash deleted when rewriting the user program in the boot mode?
Latest Updated:09/11/2012
Question:
Is the data flash deleted when rewriting the user program of the on-chip flash memory in the boot mode?
Answer:
In the boot mode and the USB boot mode, the data flash (data MAT) will be completely deleted at the time of activation.
Suitable Products
SH7214, SH7216 |
SH7231 |
SH7239, SH7237 |