What value to set to CKS of the SCSMR and to SCBRR when using SCI?
Latest Updated:03/21/2012
Question:
When using SCI in asynchronous mode with an external clock input, what value should I set to CKS of the SCSMR, and to SCBRR?
Answer:
No specific setting is required for CKS of the SCSMR and SCBRR when using them with external clock input.
Suitable Products
SH7285, SH7286 |
SH7243 |
SH7214, SH7216 |
SH7239, SH7237 |
SH7211 |
SH7124, SH7125 |
SH7146, SH7149 |
SH7083, SH7084, SH7085, SH7086 |