Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Usage of TPS-1 TPS_Target_Debug Image

Last Updated:06/01/2017

Question:

How do I use the image TPS_Target_Debug.img?

Answer:

The TPS_Target_Debug.img file is used to load the debug version of the PROFINET stack into the serial flash of the TPS-1. This debug version provides extended outputs via the TPS-1 UART. It is typically used during development and it cannot be used for the PROFINET certification and final product.
Suitable Products
TPS-1