Skip to main content
Knowledgebase
Home
Renesas Electronics America - Knowledgebase

Can Renesas Provide PROFINET Certification

Last Updated:06/02/2017

Question:

Can Renesas provide PROFINET certification?

Answer:

No, but the certification process is supported by regional certification labs that are accredited by the PROFIBUS and PROFINET International (PI) organization.
Suitable Products
TPS-1
  • Was this article helpful?